web counter

An Overview of SD Card

Published: 12 April 2021 | Last Updated: 12 April 202112706
The SD (Secure Digital) card is a new generation of memory devices based on semiconductor flash memory. Due to its small size, data transmission speed, hot-swap, and other excellent features, it is widely used in portable devices, such as digital cameras, tablets, and multimedia players, etc.
SD card speed classes, bus interfaces, capacity types and application classes explained, including information on the forthcoming SD Express and SDUC.

Explaining SD Cards

Catalog

Ⅰ Overview
Ⅱ SD card characteristics
Ⅲ SD card structure
Ⅳ SD mode
Ⅴ SD card derivatives
Ⅵ SD card specifications


Ⅰ Overview

SD memory card is a new generation of high-speed storage devices based on semiconductor fast flash memory. The technology of the SD memory card is derived from the MULTIMEDIA Card format, and it has developed SDIO (SD Input/ Output) card on the basis of a compatible SD memory card. This compatibility includes mechanical, electronic, electricity, signal, and software. SD cards and SDIO cards are usually called SD memory cards.

The SD card has high memory capacity, fast data transmission rate, great mobile flexibility, and good security, which are widely applied to portable devices, such as digital cameras, tablets, and multimedia players. 

The SD card structure ensures the security of digital files, and it is also easy to reformat, so there is a wide range of applications. Multimedia files such as music, movies can be easily saved to the SD card. There are many brands of SD cards on the market such as SanDisk, Kingmax, Panasonic, and Kingston. 

SD card is a new type of storage device with the following features: 

● High storage capacity, most common capacity: 8GB, 16GB, 32GB, 128GB, 256GB, etc.

● Built-in encryption technology adapts to the copyright protection function based on the SDMI protocol.

● High-speed data transfer; maximum read and write rate is 100Mb / s.

● Light size, easy to carry, with strong impact resistance.

Ⅱ SD card characteristics

The digital copyright protection scheme embedded in the SD card is set according to the Content Protection for Recordable Media (CPRM) proposed in 4C. Its core is the use of the Cryptomeria password (also known as "C2"). This feature is confidential. The DVD-AUDIO CD also uses an encryption scheme that is very similar to CPPM. SD card (Secure Digital Memory Card) is a new generation of memory devices based on semiconductor flash memory. SD card jointly developed its development in Panasonic, Toshiba, and SanDisk in Toshiba and SanDisk in June 1999. The size is like a stamp's SD memory card, with only 2 grams, but has high memory capacity, fast data transmission rate, great mobile flexibility, and good security. 

The SD card combines SanDisk flash memory card control and MLC (Multilevel Cell) technology and Toshiba 0.16U and 0.13U NAND technology. It is connected to a special drive through a 9-pin interface and does not require an additional power supply to keep the information memorized on it. Moreover, it is an integrated solid medium, there is no moving portion, so there is no need to worry about damage to mechanical movement. 

The biggest feature of SD cards is to ensure the security confidentiality of data by encryption. The SD card is consistent with the MultiMedia card on the shape and is compatible with the MMC card interface specification. However, some products such as mobile phones, SD cards, and MMS cards cannot be compatible. The SD card is higher than the equivalent MultiMedia Card card in terms of selling. 

SD card is used for MP3 Walkman, digital camera, digital camera, etc. Its projection area is the same as the MMC card, but the capacity of the SD card is much larger, and the read and write speed is also 4 times faster than the MMC card. At the same time, the interface of the SD card is compatible with the MMC card, supporting the SD card interface to support the MMC card. In 2013, the SD card was rapidly popular in digital cameras, and it became mainstream. The SD card has developed rapidly in 2013 and has begun to threaten the market share of the CF card. This is because the size of the SD card is much smaller than the CF card, and the SD card is getting smaller and smaller in capacity, performance, and price, and the gap between the CF card. The rapid growth of the SD card is definitely not accidental. The most important thing is that the MMC card can also be compatible with SD cards, which is also one of the reasons for SD cards.

Ⅲ SD card structure

In addition to the 7 needles of the MMC card, the SD card interface is also added to the two edges, as the data line. 

In the SD card 3.0 specification, the maximum capacity of the SD card can reach 2TB. The theory's maximum read and write speed can reach 104MB / s (in the latest 4.10 specification, the theoretical maximum read and write speed has increased to 312MB / s). 

SD card structure

SD card structure

The SD card is mainly divided into four parts: external pins, internal registers, interface controllers, and internal storage media. 

Pin

The main pins and functions of the SD card are as follows: 

CLK: Clock signal, controller, or SD card transmits a command bit or data bit in each clock cycle. The frequency can vary between 0 to 25 MHz in the default speed mode of the SD bus, and the bus manager of the SD card freely produces a frequency of 0 to 25 MHz. In the UHS-I velocity mode, the clock frequency can be up to 208m. 

CMD: Command and Response Reader, the command is sent by the controller to the SD card, which can be from the controller to a single SD card, or all the cards on the SD bus. The response is the command sent by the memory card Answer, the response can come from a single card or all cards. 

Dat0 ~ 3: Data cable, data can also be transferred from the controller to the card from the card. 

Register 

The register and its functions are described below: 

OCR (OPERATING CONDitions Register): 32-bit operating condition register mainly stores the VDD voltage range, and the SD card operating voltage range is 2 ~ 3.6V. 

CID (CARD Identification Register) Register: The card identification code register, the length is 16 bytes, and the SD card unique identification number is stored. This number cannot be modified after the card manufacturer is programmed. 

CSD (Card-Specific Data Register) Register: The Carter Data Register contains the necessary configuration information when accessing the card data.

SCR (SD CARD Configuration Register): SD Card Configuration Register (SCR) provides some special features with the SD card which are 64 bits, and this register content is set by the manufacturer. 

RCA (Relative Card Address) Register: The card relative address register is a 16-bit writable address register. The controller can select the SD card corresponding to the address by the address.

DSR (Driver Stage Register) Register: Drive Level Register, which belongs to an optional register for configuring the drive output.  

Interface controller

Mainly used to control and manage the core of the internal storage, by receiving the commands sent by the user to control and set, and respond according to the command, and then perform the response data read/write and other operations. 

Internal storage medium

Data memory stored Flash block.

Ⅳ SD mode

Drive mode

The SD card has two drive modes: SPI mode and SDIO mode. The interface signals they use are different. In SPI mode, only 4 signal lines of the SD card, ie CS, DI, SCLK and DO (sd card selection, data input, clock, and data output). 

Transmission mode

SD card supports three transmission modes: SPI mode (independent sequence input and sequence output), 1-bit SD mode (independent instruction, data channel, unique transmission format), 4-bit SD mode (using the additional pin and certain Reset the pin. Supports four-bit width parallel transmission).

Low-speed cards typically support 0 to 400 kilobits / second data transfer rates, using SPI and 1-bit SD transmission mode. The high-speed card supports 0 ~ 100 megabits/sec data transmission rate, using 4-bit SD transmission mode; support 0-25 megabits/sec, SPI, and 1-bit SD mode. 

Manufacturers, vendors, and host adapter manufacturers need to pay SD / SDIO licensing fees, plus $ 1,000 per year to 1,500 US dollars. However, the SDIO card and MMC adapter manufacturers do not have to authorize fees. The MMC card uses a 7-pin interface, the SD card, and the SDIO card use a 9-pin interface.

Ⅴ SD card derivatives

MINI SD card

MINI SD was developed by Panasonic and SanDisk. The first appearance was in the SanDisk booth in the 2003 CEBIT exhibition. Since then it has added Memory Stick Duo and XD cards such as a small memory card specification. 

The design of the MiniSD card is initially made to take pictures with a photo pine mobile phone. 

It can also be used as a general SD card by the SD adapter card. 

The capacity of the MiniSD card is from 16MB to 8GB, while the capacity of the MiniSDHC card is from 4GB to 16GB. 

sizes of different SD card

sizes of different SD card

Micro SD card

On the ultra-small memory card product, the SD Association took the lead in incorporating T-Flash into its family and named Micro SD to replace the status of Mini SD.

Only after the nail size Micro SD has been amazed after the launch of 2005. In 2008, the phone has spread this very small memory card. 

M2, Micro SD, and MMC Micro are listed in the world's smallest mini memory card, and the ultra-small volume has a greater advantage. It can be applied to various types of digital products. For exquisite digital life, it has also played the role of "promoting wave". It is unfortunately only MICRO SD that only survives. The M2 card is a Sony version of Micro SD, eventually replaced by Micro SD. 

Ⅵ SD card specifications

Rate level

"X" representation (SD1.0 specification, not used now):

It is calculated from the 150kb / s of the CD-ROM to a 1-fold speed calculation method. Basically, they can be 6 times faster than the standard CD-ROM (900 kB/sec), while the high-speed SD card can transmit 66X (10 MB / sec) and 133x or higher speed. Some digital cameras require high-speed SD cards to shoot more smoothly, and continuous shooting photos more quickly.

Up to December 2005, most of the equipment followed from the SD card 1.01 specification, and the higher speed to 133X equipment also followed from 1.1 specifications, up to 12.5MB / sec.

SD2.0 specification:

The rate of ordinary cards and high-speed cars is defined as class2, class4, clas6, and class 10 levels. Before the Class 10 card, there is a card that has Class11 and Class13, but this standard is eventually not a consensus with the SDA. 

SD3.01 specification:

Also known as the ultra-high-speed card, the rate is defined as UHS-I and UHS-II. By the second quarter of 2013, only the UHS-I card has been listed. UHS-II was released in the fourth quarter of 2012, but in terms of technology development before 2014, UHS-I was complete enough to spend 2014 or even longer. The speed level of the UHS-I card is divided into UHS-Class0 and UHS-Class1. The Class and SD2.0 of the UHS-i are different, and there is no clear Class0 card, and the literal meaning is the card that does not reach Class1. It may be summarized as Class0 in the future. Class1 represents the maximum read of 104MB / s, while the Class represents the SD2.0 standard represents the smallest speed range.

The marker symbol on the card is shown in Figure.

Rate level symbol on the card

Different levels of reading speed and application requirements that meet:

Different levels of reading speed and application requirements

Capacity level

The SD card capacity is currently three levels, that is, SD, SDHC, and SDXC. 

The table below is the level capacity range and standard disk format:

Level capacity range and standard disk format

The SD capacity is 8MB, 16MB, 32MB, 64MB, 128MB, 256MB, 512MB, 1GB, 2GB.

The SDHC capacity has 2GB, 4GB, 8GB, 16GB, 32GB.

The SDXC capacity has 32GB, 48GB, 64GB, 128GB, 256GB, 512GB, 1TB, 2TB.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is an SD card used for?

An SD card, short for Secure Digital card, is a type of removable memory card used to read and write large quantities of data in a wide variety of mobile electronics, cameras, smart devices, and more.

2.What mean SD?

Secure Digital  SD (Secure Digital) cards are the oldest and least-used and are limited to 2 GB of storage. SDHC (High Capacity) cards can store up to 32 GB of data.

3.Can an SD card die?

But just like external hard drives and other storage devices, SD cards are prone to severe damage and failure. They have a limited lifespan and with each passing day, the chances of getting corrupted increase. SD cards should be kept in proper cases when not put in the device.

4.What happens if you put someone else's SD card in your phone?

Yes, it will work 100% fine, especially if it's from another Android phone and you're putting it instead of a different Android phone. The micro SD cards can be read by any device pretty much, and nothing bad will happen.

5.Which is better SD SDHC or SDXC?

SDHC (high capacity) cards can store up to 32 GB of data, while SDXC (extended capacity) cards can store up to 2 terabytes (2000 GB). Older devices may not be able to use the SDXC format, so make sure your device does support these larger cards before buying one.

6.What are the best micro SD cards in 2021?

SanDisk Extreme A2 256GB.   Kingston Endurance microSD 128GB.   Samsung Evo Select 128GB.   SanDisk MicroSD Nintendo Switch 256GB.   Integral UltimaPro 128GB.   Kingston Canvas React Plus V90 Card.   Samsung Pro Endurance 64GB.   Pioneer Premium 128GB microSD.
Related Articles

  • High-Capacity HDDs in the AI Era: Sourcing Massive Storage for Cold Data
    High-Capacity HDDs in the AI Era: Sourcing Massive Storage for Cold Data
    UTMEL04 July 2026786

    As generative AI and LLMs drive an explosion of unstructured data, high-capacity enterprise HDDs remain the most cost-effective solution for cold storage. Despite rising prices and supply chain bottlenecks, mechanical drives offer a massive cost-per-gigabyte advantage over SSDs. Technologies like HAMR and SMR enable capacities beyond 24TB, though deploying these drives requires robust RAID 6 strategies and secured IC supply chains to mitigate rebuilding and procurement risks.

    Read More
  • LPDDR5 Memory 2026: Lead Times, HBM Impact, and Procurement Strategies
    LPDDR5 Memory 2026: Lead Times, HBM Impact, and Procurement Strategies
    UTMEL17 July 20265025

    Global semiconductor fabrication facility managing advanced memory production. In Q2 2026, contract prices for 12GB LPDDR5X modules surged 89% quarter-over-quarter, jumping from $77.10 to $145.90, while lead times for advanced memory components stretched to 40–58 weeks. A vehicle platform designed in 2023 with specific memory requirements must ship in 2026, regardless of spot market conditions.

    Read More
  • 2026 DRAM and the 3-to-1 HBM Rule: Market Supply Analysis and B2B Procurement Guide
    2026 DRAM and the 3-to-1 HBM Rule: Market Supply Analysis and B2B Procurement Guide
    UTMEL23 July 20266444

    This technical report explains how the physical "3-to-1 wafer penalty" of High Bandwidth Memory (HBM) production has cannibalized standard DRAM capacity, causing severe shortages of DDR4 and DDR5 in 2026. As major hardware OEMs pass these soaring component costs directly to enterprise buyers, procurement teams must abandon Just-in-Time models in favor of rolling safety stocks and strategic long-term distributor agreements to protect budgets.

    Read More
  • Automotive vs. Industrial Memory: How to Verify Grade Codes Before Sourcing In this guide
    Automotive vs. Industrial Memory: How to Verify Grade Codes Before Sourcing In this guide
    UTMEL06 August 2026602

    Memory ordering codes can look almost identical while representing different temperature limits, packages, revisions, qualification evidence, or lifecycle commitments. For automotive and long-life industrial designs, the safe purchasing unit is the complete manufacturer ordering code, not a base part number plus a familiar-looking suffix.

    Read More
  • How to Use an External Hard Drive?
    How to Use an External Hard Drive?
    UTMEL24 June 20219534

    The external hard drive is a compact and portable hard drive storage which can be plugged in or unplugged at any time. It mainly uses USB or IEEE1394 interfaces. It can transmit data with the system at a higher speed. The IEEE 1394 interface transfer rate is 50-100 MB/s.

    Read More

Subscribe to Utmel !

Featured Parts More